Archives de la catégorie : Strand-Fill in Medium Voltage Tape Shield Cable

Benefits and Arguments of Strand Fill in Conductors

Flux RSS de Strand-Fill in Medium Voltage Tape Shield Cable

Dernière mise à jour le .

Strand-fll sometimes called moisture-block is a tar like substance that is applied between each lay-er of a concentric stranded copper or aluminum phase conductor. During the stranding process and at slightly elevated temperatures this tar like substance becomes fuid enough to be forced through a pump and applied geometrically in such a manner that the interstitial space between every strand is flled with the tar. The tar is then allowed to cool whereas it becomes stable and remains in place.

Download PDF copy